Kollmorgen UDFBs

A KollmorgenUDFBClosed"User Defined Function Block" UDFB can be used as a sub-function block in another program of the application. It is described using FBD, LD, ST or IL language. Input / output parameters of a UDFB (as well as private variables) are declared in the variable editor as local variables of the UDFB is a pre-defined function block created by Kollmorgen to simplify certain tasks or demonstrate a particular function. A Kollmorgen UDFBClosed"User Defined Function Block" UDFB can be used as a sub-function block in another program of the application. It is described using FBD, LD, ST or IL language. Input / output parameters of a UDFB (as well as private variables) are declared in the variable editor as local variables of the UDFB must be instantiated before it may be used. The code inside a Kollmorgen UDFB can be modified by creating an unlocked copy in the subprogram section in the project tree..

Name  Description 
FB_AKDFltRpt Outputs AKD fault information
FB_AxisPlsPosModulo Used for any position of a modulo axis in both directions
FB_AxisPlsPosNoModulo Used for any position of a non-modulo axis in both directions
FB_Cylinder Control a cylinder and the Limit Switches.
FB_ElapseTime Keeps track of the time that a Boolean input variable is on.
FB_FirstOrderDigitalFilter Filter an Analog signal.
FB_PWDutyOutput Converts an input range to a duty cycle percentage
FB_S700FltRpt Outputs S700Closed"Servostar 700 drive" See Servo Drive in Glossary drive fault Information
FB_ScaleInput Scale DINT to LREAL
FB_ScaleOutput Scale DINT to LREAL
FB_TemperaturePID  Provides PIDClosed"Proportional-Integral-Derivative" A PID controller is a generic control-loop feedback mechanism widely used in industrial control systems. An "error" occurs when an event or a disturbance triggers off a change in the process variable. A PID controller attempts to correct the error between a measured process variable and a desired setpoint by calculating and then outputting a corrective action that can adjust the process accordingly temperature control with auto tuning
MCFB_AKDFault Outputs AKD drive fault Information.
MCFB_AKDFaultLookup String message of the corresponding AKD drive fault number
MCFB_GearedWebTension Facilitates dancer and tension control in an electronic geared master/slave machine design
MCFB_Jog Jog an axis in the selected direction at a defined speed
MCFB_StepAbsolutes Performs a static homing function by setting Actual Position to the position of an absolute encoder
MCFB_StepAbsSwitch Performs a homing function by searching for an absolute positioned external physical switch
MCFB_StepAbsSwitchFastInput Performs a homing function by searching for an absolute positioned external physical switch
MCFB_StepBlock Performs homing against a physical object, mechanically blocking the movement
MCFB_StepLimitSwitch Performs a single-axis home to a limit switch
MCFB_StepLimitSwitchFastInput Performs a homing function by searching for an external physical switch
MCFB_StepRefPulse Performs homing by searching for Zero pulse, Marker, or reference pulse in encoder
MLFB_HomeFindHomeFastInput Performs a single-axis home to a limit switch connected to a High Speed Input
MLFB_HomeFindHomeFastInputModulo Performs a single-axis home to a limit switch connected to a High Speed Input
MLFB_HomeFindHomeInput Fast HomingClosedThe Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position to a home switch
MLFB_HomeFindHomeInputThenZeroAngle Fast Homing to a home switch + Zero angle
MLFB_HomeFindLimitFastInput Homing to a limit switch
MLFB_HomeFindLimitFastInputModulo Homing to a limit switch: Modulo mode
MLFB_HomeFindLimitInput Homing to a limit switch
MLFB_HomeFindLimitInputThenZeroAngle Homing to a limit switch + Zero angle
MLFB_HomeFindZeroAngle Homing to a zero-angle reference
MLFB_HomeMoveUntilPosErrExceeded Homing until the position error is exceeded
MLFB_HomeMoveUntilPosErrExceededThenZeroAngle Homing until the position error is exceeded + Zero angle
MLFB_HomeUsingCurrentPosition Homing using the current position
MLFB_Jog Jog in a selected direction at a defined speed
MLFB_PlsPosFw Forward position range indicator
MLFB_PlsPosFwBw Forward/Backward position range indicator
MLFB_PlsTimeFw Forward/Backward position/time range indicator
PipeNetwork_FFLD  Used to call the PNCode function block in FFLD POUs
ProfilesCode_FFLD  Used to call the ProfilesCode function block in FFLD POUs

Table 8-51: List of System Kollmorgen UDFBs

How to create an instance

An instance of the UDFB has now been created in Subprograms.


  • You cannot create the instance of the UDFB directly from the dictionary or from the PLC Editor.

Working with Kollmorgen UDFBs

By default all Kollmorgen UDFBs are protected, meaning they may not be modified or renamed. When a Kollmorgen UDFB is dropped into an instance it is not editable. There are two solutions to make it editable:

  • Right click on a Kollmorgen UDFB that has been dropped into an instance (in Subprograms) and select Unlock. This creates an unlocked version of the UDFB with the name "U<sequence number><UDFB name>".

  • Instead of dropping a Kollmorgen UDFB into an instance, right click on the UDFB and select Create unlocked copy in Subprograms. This creates an unlocked instance of the UDFB with the name "U<sequence number><Kollmorgen UDFB name>".

Once a Kollmorgen UDFB has been unlocked it may be renamed and exported by right-clicking on the UDFB. Renamed UDFBs must have unique names. Importing a saved UDFB will increment the UDFB's name.


  • In order for a UDFB to modify a structure or array based on the output, you must first define it as an input. The input is automatically set as an INOUT parameter. This is because OUTs are strictly simple types.